Part Number: TMDSEVM6678
I ran an example of multicore communication and compiled it showed the following error:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSEVM6678
I ran an example of multicore communication and compiled it showed the following error:

Are you able to successfully build the other PDK examples? or this is the first example you are trying out?
Is this example, your own creation using CCS?
If yes, I would recommend you to first run the existing examples of processor SDK of C6678 and have a hands-on and then move on to the own.
--
And also, request you not to create multiple threads on the same topic.
---
FAQ to generate the PDK examples : - [FAQ] TMS320C6678: How to generate the CCS PDK examples for C6678? - Processors forum - Processors - TI E2E support forums
How to build and run the UART example: - [FAQ] TMS320C6678: UART Example project for C667x family devices - Processors forum - Processors - TI E2E support forums
How to run the platform test :- [FAQ] TMS320C6678: How to build and run the platform test on C6678 EVM ? - Processors forum - Processors - TI E2E support forums
Qick start guide for C6678 EVM: -[FAQ] TMS320C6678: Quick set up Guide C6678 and C6678-EVM - Processors forum - Processors - TI E2E support forums
Regards
Shankari G