Hello,
I have a data file that is in intel-hex format. Do i need to convert that to C code? Or can i upload the hex files directly through CCS? If so, Please tell the procedures of getting the data loaded (which is in intel hex format) into CCS.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have a data file that is in intel-hex format. Do i need to convert that to C code? Or can i upload the hex files directly through CCS? If so, Please tell the procedures of getting the data loaded (which is in intel hex format) into CCS.
Thanks Lisa. I'm using MSP-EXPFR5739 and also the data is in tabular format not executable code.
Hi Harika,
what format exactly do you have? Is it intel hex?
If it is intel hex or TI .txt format, then actually you are best off to use a free recommended flash programmer from Elprotronic (www.elprotronic.com)
I will look into the possibilities directly in CCS, but would need to know are you using 4.2 or 5.1? In any case, it will not be the elegant solution.
Cheers,
Lisa
Yes, Intel hex format and if not i can have that converted to binary format too. And the version i'm using is CCS 4.2.3
Thanks Lisa, looking forward for your solution.
Hello again Harika,
ok, there actually for those formats are no CCS options. The best, as mentioned, is to use the free Elprotronic tool (www.elprotronic.com).
You may find the following information helpful as well.
http://processors.wiki.ti.com/index.php/Generating_and_Loading_MSP430_Binary_Files
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/42268/148106.aspx#148106
http://processors.wiki.ti.com/index.php/Loadti#Debugging_Your_Changes_to_loadti
I hope this helps. Sorry there is not a more elegant solution, but because Elprotronic has such a nice tool, it seems it was seen as reproduction to have the same thing in CCS.
IAR can load a hex file, if you really still wish for a compiler environment.
Best Regards,
Lisa