Other Parts Discussed in Thread: OMAPL138
Hi,
I am a newbie to TI processors.
I was trying to run the NSP demo "ndk_evm6748_bios5_cfgdemo" in Spectrum Digital EVM6424 board.
I have tried the following changes to make the demo run in 6424.
C/C++ Build->c6000 Compiler->Basic Options->Target processor version :: 64+ instead of 6740
In C/C++ Build->c6000 Linker->File Search Path, everything is changed to ${NDK_INSTALL_DIR}/packages/ti/ndk/lib/C64plus instead of ${NDK_INSTALL_DIR}/packages/ti/ndk/lib/C674. But still there is no alternative for "${NSP_INSTALL_DIR}/packages/ti/drv/omapl138/lib/debug/ti.drv.omapl138.a674"
In CCS Build, Device variant is selected as "Generic C64x+ Device".
After building i tired to start a debug session, the error came was
Failed to load program 'ndk_evm6748_bios5_cfgdemo.out' on target 'Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator/C64XP_0'
Reason: Invalid file format.
Could anyone please point out what are the major modifications needed to run the NSP in c6424.
Thanks,
Ragesh