This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

connecting to ARM and DSP of OMAP L138 with xds100v2,CCS V4.2

Other Parts Discussed in Thread: OMAP-L138, OMAPL138

Hi,

  I'm trying to debug / run the message queue sample application of OMAP L138 ( LogicPD experimenter kit)

I've followed the steps as per http://processors.wiki.ti.com/index.php/How_to_connect_to_the_OMAP-L138/C6748_EVM_board_using_CCS%3F

In the step,creating target configuration file,i've selecting the ARM,DSP gel files which is downloaded from logicpd.when i try to save the .ccxml i'm getting error

line :                <device HW_revision="1" XML_version="1.2" id="OMAPL138 - ARM9 and C674x Floating point DSP_0" partnum="OMAPL138">

error msg: cvc-complex-type.4:Attribute 'description' must appear on element 'device'

 

Let me know any other link available for multicore debugging for OMAP L138 with sample application.

Thanks

Arul.