This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have created a software breakpoint to a specific line of source code and printed out its properties (see below) however there doesn't appear to be any reference to the relevant program address (for other breakpoint types I would compare this with the value of the program counter as per examples). Therefore, is there any way to tell (using DSS/GEL) that I have actually reached the correct breakpoint?
|=================================================================================================================
| TYPE: Software
| ID: 16
|-----------------------------------------------------------------------------------------------------------------
| PROPERTY VALUE ALLOWED VALUES
| -------- ----- --------------
| Hardware Configuration.Location
C:/CodeComposer/Software/MyModule/mySource.c, line
36
| Debugger Response.Condition
| Debugger Response.Skip Count 0x0
| Debugger Response.Skip Count.Current Count 0x0
| Debugger Response.Action
Remain Halted Update View, Refresh All Windows, Control
Profiling, Execute Expression (GEL), Enable a Group, Disable a Group,
Read Data from File, Write Data to File, Remain Halted
| Miscellaneous.Group Default Group Default Group
| Miscellaneous.Name
|=================================================================================================================
Thanks,
--
Joshua
Hi Lisa,
Thanks very much for your assistance; much appreciated.
Yes, previously all of my breakpoints have been to known addresses (usually extracted from the symbol itself).
Cheers,
--
Joshua
By the way, just for more information, the reason that I am using this method rather than just taking the actual program address directly from the Disassembly view is that otherwise I receive the error "Insufficient resources" (I think the number of HW breakpoints is rather limited on my target, the MSP430F249).
Hi Joshua,
sorry again for the time here but I have a lot to learn myself.
From what I can tell when you do a printProperties it only prints out items as that that were specifically set. Unfortunate but I don't believe in your case there is a work around.
All the best,
Lisa