This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with inline function in cgtools 6.1.11 (target tms320c6727)

Hello, ALL!!!

We are going transit from 5.3.0 version of cgtools to 6.1.11.
We compile our code using cgt 6.1.11 and saw that it is work slower that compiled using 5.3.0. In both cases compilation keys were the same.

We investigate the problem and found out that version 6.1.11 made less inlined functions according to optimization report. Optimization level is -O3. Report is generated using -on2 key for both version of compiler. But we have no direct evidence that the reason of slower work is inlined functions.

Can you help us to clarify the issue?
Thank you in advance.

Best regards

 

  • hi,

    Do you have a loop into eratta sheet for 6_1_11 version of compiler ?

    If i remember correctly there is a bug in compiler 6.1.11 for inlined function. I have to dug up my mails to correctly point out the bug in 6.1.11

    Br