Part Number: LP-MSPM0G3507
Hi, I'm working with the LP-MSPM0G3507 (rev. 1.0) board.
I'm trying to implement CAN communication; I need to transmit the data through CAN with this board. I'm trying with example code, single and multiple msg tx, but not able to get data.
As this is old version of board, here no high frequency clk in this board, so I'm using PLL with 40MHz frequency.
I connected the CAN transceiver IC as well.
But still, I'm not able to get data in PCAN.
Please help me with this.
Thanks, and Regards
Abhaya Raj Mishra