Part Number: LP-MSPM0G3507
Other Parts Discussed in Thread: MSPM0G3507
Tool/software:
Hello guys,I am new coding in CCS with using MSPM0G3507. I want to create a simple Led blinking program with using external button and a resistor but I cant create .out,project.o and project.d files as well ticlang.d and ticlang.o: could zou help me to create mz first program?Below there is mz code.
#include "ti_msp_dl_config.h"
#include <C:/Users/ta/workspace_v12/test1/Debug/include/msp/m0p>
extern volatile uint32_t interruptVectors[];
int main(void)
{
SYSCFG_DL_init();
/*
* Turn OFF LED if SW is open, ON if SW is closed.
* LED starts OFF by default.
*/
NVIC_EnableIRQ(GPIO_SWITCH_INT_IRQN);
DL_GPIO_clearPins(GPIO_LEDS_PORT, GPIO_LEDS_PIN_0_PIN);
while (1) {
__WFI();
}
}
void GROUP1_IRQHandler(void)
{
switch (DL_Interrupt_getPendingGroup(DL_INTERRUPT_GROUP_1)) {
case GPIO_SWITCH_INT_IIDX:
/* If SW is high, turn the LED off */
if (DL_GPIO_readPins(
GPIO_SWITCH_PORT, GPIO_SWITCH_PIN_1_PIN)) {
DL_GPIO_clearPins(GPIO_LEDS_PORT, GPIO_LEDS_PIN_0_PIN);
}
/* Otherwise, turn the LED on */
else {
DL_GPIO_setPins(GPIO_LEDS_PORT, GPIO_LEDS_PIN_0_PIN);
}
break;
}