Team,
Go the following feedback on CCSv5 Linux:
Question on emulating legacy C64x devices with CCSv5 on LINUX:
Up to now it seems that the following two combinations up and running:
- Win XP, CCS v4, XDS560v2, TMS320C6412
- Win XP, CCS v5, XDS560v2, TMS320C6412
What still doesn't work is CCS v5 under Linux.
When I try to set up the same target configuration, I get an error message:
"Unable to find an appropriate device driver for connection type TIXDS560 and C6412"
Other emulators also don't support C64xx. The only working combination is a simulator.
It seems there are no Linux drivers at all for the C64xx CPU family.
Are such drivers are available or will be available in future?
Thanks and best regards,
Anthony