This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
When i build my project i have the following errors.
--------------------------
Error, Don't know how to build file "C:\CCStudio_v3.3\boards\evmdm6437\lib\evmdm6437bsl.lib"
Error, Don't know how to build file "C:\dvsdk_1_11_00_00\examples\common\evmDM6437\i2c_params.c"
Error, Don't know how to build file "C:\Projects\InlineStab\DM6437\d3.cmd"
Error, Don't know how to build file "C:\Projects\InlineStab\DM6437\main.c"
Error, Don't know how to build file "C:\Projects\InlineStab\lib\edma3_drv_bios_sample.lib"
Error, Don't know how to build file "C:\Projects\InlineStab\src\compute_motion.c"
...
Build Complete,
31 Errors, 0 Warnings, 0 Remarks.
(also all my *.c and *.h and lib files are not showed in the project file tree.)
-----------------------------
i also went
(1) ('Help->About->Component Manager'), expand the 'Texas Instruments, Inc' node and found that the Project Management component is enabled.
(2) "CCS-> Help-> About (it should show the CGT version). Click on Component Manager, Expand Build tools for TMS320C64XX and found that CGT is selected.
Please give me some help.
Thanks a lot,
-shunguang
Shunguang,
Have you download the DM6437 DVSDK and install? It is located at:
http://processors.wiki.ti.com/index.php/TMS320DM6437_DaVinci_Technology_One-Day_Workshop
Regards,
Viet
Hi Viet,
Thanks for replying. i installed that part. The following is our environment set up instructions, any comments on that?
Thanks,
-shunguang
-------- How To Setup Building Environment --------------
0) SW package locations: \\stingray01\ps01\Tools\Ti
1) Install CCStudio v3.3 (only works for WinXP, for Win7, need CCStudio v4.0)
(a) \\stingray01\ps01\Tools\Ti\Download\evmDM6437_CD\ccs
2) Setup SDK (\\stingray01\ps01\Tools\Ti\Download)
Install DV SDK 01_11_00_00 by running
(a) DM6437_DVSDK_setupwin32_1_11_00_00.exe
(b) EDMA3_LLD_setupwin32_01_10_00_01.exe
//-------------------
2) Install DM6437 EVM (\\stingray01\ps01\Tools\Ti\Download\evmDM6437_CD\Launch.exe)
(a) Install Products -> DM6437EVM Driver and target contents
//----------------
4) goto C:\CCStudio_v3.3\board\evmdm6437_v2, rename folder “evmdm6437_v2” to “evmdm6437”
5) start->all programs->Taxes Instrument->component Mgr (by click)
"code composer Studio v.3.3x.x" ->target contents(DSP/BIOS) -> TMS320C64xx -> check 5.31.07 version(?)
7) set win environment variable (??)
set BIOSUTILS_INSTALL_DIR as "tall_dir ->07
8) Install Blackhawk JTAG DISK
a. Install emulator driver
b. Pick USB560bp jtag emulator
c. Pick CCStudio v3.3 (run check first)
d. Pick “usb560bp jtag emulator only ? select 560/.. port
(Then click install. After install it, do step e)
e. Put emulator usb in pc: no window search and automatic
(the verify by step f)
f. Start blockhawkControl icon on Desktop
9) Set CCStudio (by run Setup CCStudio V3.3)
a. Remove all others on left
b. Platform ->bh_usb560 (for 642), (for 6437 bh_usb560(bp))
c. Family ->C64xx (for 642), (for 6437 C64x+)
d. Pick DM640,1,2,3 (for 642), (for 6437 DM643x)
e. << add on bottom
f. Save and quit. Yes to start composer studio
Yes, i have the following complaint when start CCstudio_v3.3
"Your code composer does not support the connected target.
Device driver name: "c:\CCstudio_v3.3\drivers\tixds560icepick_c.dvr"
Shunguang,
I am going to move your thread to CCS so some one can help you with that problem. I think you need the driver for that JTAG but I don't know where to get it.
Regards,
Viet
shunguang wu said:Hi all,
When i build my project i have the following errors.
--------------------------
Error, Don't know how to build file "C:\CCStudio_v3.3\boards\evmdm6437\lib\evmdm6437bsl.lib"
Error, Don't know how to build file "C:\dvsdk_1_11_00_00\examples\common\evmDM6437\i2c_params.c"
Error, Don't know how to build file "C:\Projects\InlineStab\DM6437\d3.cmd"
Error, Don't know how to build file "C:\Projects\InlineStab\DM6437\main.c"
Error, Don't know how to build file "C:\Projects\InlineStab\lib\edma3_drv_bios_sample.lib"
Error, Don't know how to build file "C:\Projects\InlineStab\src\compute_motion.c"
...Build Complete,
31 Errors, 0 Warnings, 0 Remarks.(also all my *.c and *.h and lib files are not showed in the project file tree.)
To manually register the dlls, open a command prompt, 'cd' to the bin directory within the codegen tools (assuming you're using the default version in CCS 3.3 it would be C:\CCStudio_v3.3\C6000\cgtools\bin), and type:
regsvr32 bti6000.dll
Similarly, 'cd' to the directory C:\CCStudio_v3.3\cc\bin, and type:
regsvr projsvr.dll
shunguang wu85006 said:i have the following complaint when start CCstudio_v3.3
"Your code composer does not support the connected target.
Device driver name: "c:\CCstudio_v3.3\drivers\tixds560icepick_c.dvr"
Do you have the full version of CCS 3.3 or one that was bundled with a DSK or eZdsp? If it is a version that was bundled with a DSK, it will not work with an external xds560 emulator. Please see this thread where a similar error is reported: http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/35113/378078.aspx#378078
To get it to work with a Blackhawk 560 emulator, you need a full version of CCS as well as drivers downloaded from Blackhawk's web site that support that emulator.
I apologize for the delayed reply. Usually the version number should help identify if it is a full version or DSK version. What does your version # say in CCS Help->About? Based on the error message "Your code composer does not support the connected target", it does seem that you have the DSK version.
Hi May,
See: http://processors.wiki.ti.com/index.php/DVSDK
For future reference, please start a new thread for a new topic instead of adding on to a very old thread.
Thanks
ki
Hi,
I am also facing the same issue. All my source files are listed under Documents folder. I am using CCS3.3 in windows7. I have tried re-registering the two DLLs, but that didnt help. Please help me resolve the issure.
Thank You,
K. shriram
Shriram,
Check your ccs_Compdb.ini file in "C:\Program Files (x86)\Common Files\Texas Instruments"
Open in a text editor. Is the contents blank?
Also note that CCSv3.3 is not officially supported in Windows 7. Some have gotten it to work but others have had various issues. If you continue to encounter issues, you may want to run it from an XP virtual machine. If you insist on running in Windows 7, take a look at these articles:
http://processors.wiki.ti.com/index.php/Using_CCS_with_Windows_Vista_and_7
https://www-a.ti.com/downloads/sds_support/ReleaseNotes/CCSv3.3VistaKnownIssues.htm
But note that there is not much support we can give you.
ki
Thanks Ki for the quick reply. I was able to get the issue resolved after following this:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/186373/678629.aspx
Thanks for the support.
Shriram