Hi,
I am trying to migrate a 3.3 project to CCSv5 and the final build is failing. The reason for the failure is that the v3.3 project has a source files list as below:
[Source Files]
Source="..\lib\lib1.lib"
Source="..\lib\lib2.lib"
Source="..\SRC\SYSTEM\file1.c"
Source="..\SRC\SYSTEM\asm1.asm"
Source="..\SRC\SYSTEM\asm2.asm"
Source="..\SRC\SYSTEM\file2.c"
Source="..\SRC\SYSTEM\asm3.asm"
Source="..\SRC\SYSTEM\file3.c"
Source="..\SRC\SYSTEM\file4.c"
Source="..\SRC\SYSTEM\file5.c"
Source="..\SRC\SYSTEM\file6.c"
Source="..\SRC\SYSTEM\obj1.obj"
Source="cmd1.cmd"
The problem is that CCSv5 is not including the precompiled source obj1.obj in the build as I can see that its globals are being reported as unreferenced at the final link stage.
How do I include such a pre-compiled obj file in the link stages for CCSv5.
Regards
Phil