This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer is working on an existing DSP project which uses DM643x Chip.
Earlier they used CCSV3.3 which compiles well in that environment, but recently migrated to CCSV5.x and when they tried to compile the same project (legacy CCSV3.3 project) it is giving the below error
#35 #error NO CHIP DEFINED (use -dCHIP_XXXX where XXXX is chip number, i.e. 6201).
Are there any careabouts to consider before they move to CCSv5.x?
For now, I have provided them the following links to check. I might be missing something or is there a better document or link that could resolve their issue?
http://processors.wiki.ti.com/index.php/Migrating_to_CCSv5
http://e2e.ti.com/support/embedded/tirtos/f/355/t/191761.aspx
Hello,
The customer can try defining the chip number in the build properties. See the below thread for more details:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/353978.aspx
Thanks
ki