This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
I've seen a visual bug when having multiple projects in one workspace.
I'm using MSPM0_SDK_2.2.0.05 and Sysconfig 1.21.0.
When multiple sysconfigs of different projects are open, making changes to one of them produces the unsave icon to all of them.
When I make edits to only gpio_toggle_output.sysconfig, there is the circle ico on all three .sysconfig files even though I have not made edits to TIDA_012043.sysconfig or adc12_max_freq_dma.sysconfig.
I'm not sure if there is something in the backend that is linking them together but the actually changes are not applied to each of the files just the icon.
Can you close other 2 syscfg and try to reopen them again?
Hi Eason,
Thanks for the response.
Again, the changes of 1 sysconfig are NOT applied to the other 2 syscfg file. So closing the files asks if I want to save and reopening them does not do anything.
This is a visual bug that does not affect the file itself, but is confusing and concerning to new users who might mistake them as being linked.
I know I will change this thread to CCS topic. I think they will give feedback if it can be solved or limited by the platform.
I can reproduce this issue. I looks like a clear bug to me. I filed a ticket for this. Tracking link: https://sir.ext.ti.com/jira/browse/EXT_EP-11980
Thank you
ki