Other Parts Discussed in Thread: CONTROLSUITE
Hello i have a problem with ccs3 + simulink
i work with Piccolo MCU controlStick [TMS320C2000 (f28027)] and i want to link matlab simulink r2011b with ccs3.3
operation system: windows xp, 32bit
after "incrementel build" i get the following problem:
1.The call to idelink_ert_make_rtw_hook, during the exit hook generated the following error:
Error while creating the project.
The build process will terminate as a result.
2.Error while creating the project.
3.Code generation cannot proceed because the following file or folder could not be found: $(DSP2802x_INSTALLDIR)\DSP2802x_common\include
the "ccsboardinfo" command shows me the right processor!
>> checkEnvSetup('ccs','f28027')
1. Checking CCS (Code Composer Studio) version
Required version: 3.3.82.13
Required for : Automation and Code Generation
Your Version : 3.3.83.19
Incompatible version detected. CCS version does not satisfy product requirements!
2. Checking CGT (Texas Instruments C2000 Code Generation Tools) version
Required version: 5.2.1
Required for : Code generation
Your Version : 5.2.1
3. Checking DSP/BIOS (Real Time Operating System) version
Required version: 5.33.05
Required for : Real-Time Data Exchange (RTDX)
Your Version : 5.33.05
4. Checking 2802x C/C++ Header Files version
Required version: 1.28 or later
Required for : Code generation
Your Version :
### Setting environment variable "DSP2802x_INSTALLDIR" to "D:\Dokumente und Einstellungen\Mechlabor\Eigene Dateien\MATLAB\piccolo_led_test_ticcs"
5. Checking Flash Tools (TMS320F2802x Piccolo(TM) Flash API) version
Required version: 1.00
Required for : Flash Programming
Your Version :
Incompatible version detected. Flash Tools version does not satisfy product requirements!
Following environment variables required for code generation could not be set:
### "FLASH_2802X_API_INSTALLDIR"
>> cc = ticcs
TICCS Object:
Processor type : TMS320C28xx
Processor name : TMS320C2800_0
Running? : No
Board number : 0
Processor number : 0
Default timeout : 10.00 secs
RTDX channels : 0
please help me i already read the similar posts in this forum.
thank you
Dennis