This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello i have a problem with ccs3 + simulink
i work with Piccolo MCU controlStick [TMS320C2000 (f28027)] and i want to link matlab simulink r2011b with ccs3.3
operation system: windows xp, 32bit
after "incrementel build" i get the following problem:
1.The call to idelink_ert_make_rtw_hook, during the exit hook generated the following error:
Error while creating the project.
The build process will terminate as a result.
2.Error while creating the project.
3.Code generation cannot proceed because the following file or folder could not be found: $(DSP2802x_INSTALLDIR)\DSP2802x_common\include
the "ccsboardinfo" command shows me the right processor!
>> checkEnvSetup('ccs','f28027')
1. Checking CCS (Code Composer Studio) version
Required version: 3.3.82.13
Required for : Automation and Code Generation
Your Version : 3.3.83.19
Incompatible version detected. CCS version does not satisfy product requirements!
2. Checking CGT (Texas Instruments C2000 Code Generation Tools) version
Required version: 5.2.1
Required for : Code generation
Your Version : 5.2.1
3. Checking DSP/BIOS (Real Time Operating System) version
Required version: 5.33.05
Required for : Real-Time Data Exchange (RTDX)
Your Version : 5.33.05
4. Checking 2802x C/C++ Header Files version
Required version: 1.28 or later
Required for : Code generation
Your Version :
### Setting environment variable "DSP2802x_INSTALLDIR" to "D:\Dokumente und Einstellungen\Mechlabor\Eigene Dateien\MATLAB\piccolo_led_test_ticcs"
5. Checking Flash Tools (TMS320F2802x Piccolo(TM) Flash API) version
Required version: 1.00
Required for : Flash Programming
Your Version :
Incompatible version detected. Flash Tools version does not satisfy product requirements!
Following environment variables required for code generation could not be set:
### "FLASH_2802X_API_INSTALLDIR"
>> cc = ticcs
TICCS Object:
Processor type : TMS320C28xx
Processor name : TMS320C2800_0
Running? : No
Board number : 0
Processor number : 0
Default timeout : 10.00 secs
RTDX channels : 0
please help me i already read the similar posts in this forum.
thank you
Dennis
Hello Dennis,
Dennis G��tz said:Required version: 3.3.82.13
Required for : Automation and Code Generation
Your Version : 3.3.83.19
Incompatible version detected. CCS version does not satisfy product requirements!
You need to check if simulink supports the version of 3.3 you have installed. Looks like it does not. You will need Mathworks to confirm this.
Dennis G��tz said:4. Checking 2802x C/C++ Header Files version
Required version: 1.28 or later
Required for : Code generation
Your Version :
### Setting environment variable "DSP2802x_INSTALLDIR" to "D:\Dokumente und Einstellungen\Mechlabor\Eigene Dateien\MATLAB\piccolo_led_test_ticcs"
Dennis G��tz said:3.Code generation cannot proceed because the following file or folder could not be found: $(DSP2802x_INSTALLDIR)\DSP2802x_common\include
Does this folder exist on your PC?
"D:\Dokumente und Einstellungen\Mechlabor\Eigene Dateien\MATLAB\piccolo_led_test_ticcs\DSP2802x_common\include"?
Thanks
ki
I believe that folder come from the 2802x peripheral examples:
http://www.ti.com/tool/sprc832
Dennis G��tz said:The next step after finding the folder, is how can i change the folder in matlab?
I don't know simulink very well but I think once you install the examples, it will be able to find the folder using an environment variable that is set when you install the examples
ki
Hello Ki-Soo,
i downloaded the 2802x peripherals examples and installed them.
now matlab find the folder but i dont have the right version: ...
Checking 2802x C/C++ Header Files version
Required version: 1.28 or later
Your Version : 1.26
Incompatible version detected. 2802x C/C++ Header Files version does not satisfy product requirements!
Following environment variable(s) required for code generation could not be set:
### "DSP2802x_INSTALLDIR"
so i think i need a greater version. can you help me one more time please.
dennis
You can get a later version from controlSUITE:
http://www.ti.com/mcu/docs/mcuproductcontentnp.tsp?sectionId=95&familyId=916&tabId=2656
Thanks
ki
Thats the answer to this problem.
After installing the controlSUITE and linking the mathlab variable "C280x_INSTALLDIR" to the ControlSuite_Dir\device_support\f2802x\v129
the Program is running on the C2000 Board :)
thanks
Dennis
(how can i verify your answer ?)
Hi,I also meet this question these days.But I don't know how to linking the mathlab variable "C280x_INSTALLDIR" to the ControlSuite_Dir\device_support\f2802x\v129 as you said.I try to creat a new systerm variable in my computer of desktop,but it dosn't work.So I holp for a more clear answer for this question.Thank you.
Hello , I'm really new using this c2000 launchpad , i recently saw that matlab can generate code for this card , i'm trying to configure if but it seems that is not working every time i get this.
Any help would be appreciated.
>> checkEnvSetup('ccsv4','f2802x')
1. Checking CCS (Code Composer Studio) version
Required version: 4.1.0
Required for : Code Generation
Your Version :
Incompatible version detected. CCS version does not satisfy product requirements!
2. Checking CGT (Texas Instruments C2000 Code Generation Tools) version
Required version: 5.2.1 to 5.2.3
Required for : Code generation
Your Version : 6.1.0
Incompatible version detected. CGT version does not satisfy product requirements!
Following environment variables required for code generation could not be set:
### "C2000_CGT_INSTALLDIR"
3. Checking DSP/BIOS (Real Time Operating System) version
Required version: 5.33.05 to 5.41.09.34
Required for : Code generation
Your Version : 6.34.02.18
Incompatible version detected. DSP/BIOS version does not satisfy product requirements!
Following environment variables required for code generation could not be set:
### "CCSV4_DSPBIOS_INSTALLDIR"
4. Checking XDC Tools (eXpress DSP Components) version
Required version: 3.16.02.32 or later
Required for : Code generation
Your Version :
5. Checking 2802x C/C++ Header Files version
Required version: 1.26
Required for : Code generation
Your Version : 1.26
### Setting environment variable "DSP2802x_INSTALLDIR" to "C:\tidcs\c28\DSP2802x\v126"
Warning: System command setx failed. System returned the following message: "reg"
no se reconoce como un comando interno o externo,
programa o archivo por lotes ejecutable.
. Manually create an environment variable DSP2802x_INSTALLDIR set to
"C:\tidcs\c28\DSP2802x\v126".
> In C:\Program Files\MATLAB\R2011b\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>setEnvVar at 581
In C:\Program Files\MATLAB\R2011b\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>envSetup at 321
In C:\Program Files\MATLAB\R2011b\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>checkEnvSetup_private at 75
In checkEnvSetup at 158
6. Checking Flash Tools (TMS320F2802x Piccolo(TM) Flash API) version
Required version: 1.00
Required for : Flash Programming
Your Version : 2.00
Incompatible version detected. Flash Tools version does not satisfy product requirements!
Following environment variables required for code generation could not be set:
### "FLASH_2802X_API_INSTALLDIR"