Other Parts Discussed in Thread: SYSBIOS
Hi,
I would like to run the excution graph features of the System Analzer.
So far I understand that functions are displayed as UIA start/stop events are available.
Questions:
Can I generate function entry/exit event without adding instrumentation code to the target ? (like log_write1(UIBenchmak_start...))
Would it be possible to run some function profiling automatically, without the need to instrument the target code ?
many thanks
Alois