This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
"Error initializing emulator:
Could not find MSP-FET430UIF on specified COM port"
Win7 64 bit
MSP430G2
I recently acquired an MSP430 launchpad and have been eager to make it work. Unfortunately, nothing seems to work. I have been trying to download a piece of code that I wrote but I keep getting the above error. I have tried using the IAR IDE,l but I also get an error similar to the above one.
I have been playing with it trying to make it work for over 7 hours but nothing has worked. Could anybody help me?
The device shows in the device manager as:
Ports (COM & LPT)
MSP430 Application UART (COM5)
and
Human Interface Devices
HID -compliant consumer control device
USB Input Device
I have actually found the problem and fixed it after doing some research. The problem happens when certain other pieces of software are running at the same time IAR or CCS is trying to compile and download the code into the MSP430 chip. In this case, the problem was solved after carefully stopping certain processes and testing whether the downloading was successful The services causing this distress were: a Dell widget application that comes with my laptop, and Daemon Tools Pro which I use to virtualize drives.
Hi Alexander,
ok, glad to hear you figured it out. All the best with development.
Best Regards,
Lisa
I had the same problem and I shut down everything that wasn't essential to they system and now it works. However I still have to hit retry 1 to 5 times to get it to work.
Thanks,
Casey
Thanks Alexander Ventura. I' ve been as well having the same debugging problem until your solution became mine. Shutting down processes one at a time came out with accuweather application interfering with debugging. so I can now work with my msp430 finally. Guys try this solution