Tool/software:
CCS version: 20.1.0
SysConfig version: 1.22.0
When a .syscfg file is opened in CCS20.1.0, the problem view, generated files view and board view are always opened by default in SysConfig, at least with the Simplelink SDK examples, that is not the case in CCS12.8.1. How do I stop these views to be opened by default?
Best regards,
Shuyang
Hello Shuyang,
This was an explicit change in behaviour as many people missed that there is additional information available when using SysConfig. However, it is good feedback to allow this configurability. I have added a ticket to allow user control over this setting. Below is the ID.
Martin
Hi Martin,
Thanks for the update and good to know the reason. I think it's great to have a configuration to control this, looking forward to the release.
Best regards,
Shuyang