I am trying to import a CCSv4 project for C2000 device (C28035) that was another engineer machine. I'm using the versions in the image below. I've used the Project Import tool by Importing an Existing CCS/CCE project and tried to Build-All and keep getting the errors described below. Is there instruciton on how to perform a "clean" import of this project and able to rebuild on my machine?
Build Error Log: See attached .txt file.
CCSv4 Errors shown in Problem Window
This project was created using a version of Code Generation tools that is not currently installed: 5.2.11 [C2000]. Please install the Code Generation tools of this version, or migrate the project to one of the supported versions.
Question: Can I get an older version of C2000 Code generation tools?
**** Clean-only build of configuration F2802x_FLASH for project 2xPM_Motors **** C:\Program Files (x86)\Texas Instruments\ccsv4\utils\gmake\gmake -k clean DEL /F "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\2xPM_Motors.out" The system cannot find the path specified. gmake: [clean] Error 1 (ignored) The system cannot find the path specified. gmake: [clean] Error 1 (ignored) DEL /F "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\2xPM_Motors-DevInit_F2803x.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\2xPM_Motors.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\DLOG4CHC.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\DSP2803x_CodeStartBranch.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\DSP2803x_GlobalVariableDefs.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\DSP2803x_usDelay.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\EcoFlowFunctions.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\EcoFlowGlobalVariables.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\VecSaturator.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\clarke.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\f2803xileg_vdc.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\f2803xpwm.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\ipark.obj" DEL /F "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\park.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\pif_reg3.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\rampgen.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\rmp_cntl.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\smopos.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\speed_est.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\svgen_dq.obj" "C:\TI_F28xxx_SysSW\HV_MotorControl_Rev1\DMC\2802x_FLASH\volt_calc.obj" The system cannot find the path specified. gmake: [clean] Error 1 (ignored) DEL /F ".\DLOG4CHC.pp" ".\DSP2803x_usDelay.pp" Could Not Find C:\CCSv4_projects\2xPM_Motors\F2802x_FLASH\DLOG4CHC.pp DEL /F ".\2xPM_Motors-DevInit_F2803x.pp" ".\2xPM_Motors.pp" ".\DSP2803x_GlobalVariableDefs.pp" ".\EcoFlowFunctions.pp" ".\EcoFlowGlobalVariables.pp" ".\VecSaturator.pp" ".\clarke.pp" ".\f2803xileg_vdc.pp" ".\f2803xpwm.pp" ".\ipark.pp" ".\park.pp" ".\pif_reg3.pp" ".\rampgen.pp" ".\rmp_cntl.pp" ".\smopos.pp" ".\speed_est.pp" ".\svgen_dq.pp" ".\volt_calc.pp" ' ' Build complete for project 2xPM_Motors