Hi all,
How can I remove the file specific build options in CCS 5.1.1?
Furthermore there seems to be a bug with folder specific build options:
When I specify the build options for a folder its icon changes but the build options I change will be used globally and vice versa, but if I change the build options for a file within this folder it seems that this is used for all files in this folder than, even if the build options for the folder are still the globally once.
Best Regards,
Christian