Hello,
I have recently converted a C2x project from CCS v3.3 to v4.2. The exercise was successful but I have found the following annoyance: my project has four configurations and when built, the output build folders appear in the project folder with the same name as the configuration. This is fine, but a little untidy. I would like a single sub-folder in the project folder called ‘Build’ and the output build folders (named as the configurations) as subfolders of this. I had this scheme working in V3.3 but cannot seem to make V4.2 do it – anyone have any ideas?
Also I, too, ran in to the problem discussed in this post:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/57598/205238.aspx#205238
This thread was ‘resolved’ by filing ‘SDSCM00037412’ (I assume some kind of bug report). Is there any further news on whether this problem has been addressed? And how? Personally, I quite like the way that v3.3 handled file specific options – by presenting them as relative changes to the standard project options. It was easy to see which options have been changed for a specific file. In CCS V4, even if the bug didn’t exist and all project level option changes where propagated down correctly, it is still hard to see which options are different for the ‘triangled’ files.
Cheers,
John.