I've recently imported a CCS 3.3 project for an OMAP l137 into CCS 4. Now when I build I get the following error:
"project_c6747cfg.s62", ERROR! at line 365: [ ***** USER ERROR ***** - ]
Project build options do not match Global configuration settings.
Compiler options do not specify -mv64+, but configuration is for
C64x+
.emsg "Project build options do not match Global configuration settings. Compiler options do not specify -mv64+, but configuration is for C64x+"
I found one other thread addressing this, but in that thread the user was on a 64+ and just hadn't set up their build options. I have my build options set to a Generic C67x+ device and the Compiler Options have the Target processor version (correctly) as a 67p.
Where is the "Global configuration" setup? I can't find anywhere that the project appears to be setup for a C64x+, yet I still have this issue.
My default Target Configuration which is used by this project is also for an OMAPl137.