This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Installed CCS today (lateste version). right before i installed eclipse from eclipse.org, also latest x86 version.
i open eclipse, and there's the CSS plugin, there's "Code Composer Studio" category in the preferences dialog (albeith without anything!)
new -> project does not show anything related to CCS.
what else should i do?
Also, will this be more productive for debugging launchpad stuff than my current msp430-gcc setup in linux? or am i just walking in circles?
Hello,
Samuele gave good advice .... simply install CCS, you do not need to install Eclipse as well or separately. If you have installed CCS over Eclipse, have a look at this wiki topic as well.
http://processors.wiki.ti.com/index.php/Installing_CCS_over_Eclipse
Best Regards,
Lisa
I should have guessed it included eclipse for the size of the archive...
anyway, i saw the checkbox to install in a existing eclipse, and thought i had to install eclipse before the install so it would already make the arrangements during install...
i now removed everything and installed from scratch and used the included eclipse install (i would me mildly annoyed if i already have a need for eclipse in this box). everything seems to be fine now. but i still have no idea why the project class didn't show up on the 1st try since everything seemed to have installed just fine.
thanks for the clarifications. i think i'm set now.