This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 5.2 crash after start debug

Other Parts Discussed in Thread: CCSTUDIO

Hi,

my CCS 5.2 crash after connecting the Spectrum Digital XDS510USB  when i start the debug session.

Please can you check the attached log files.

1805.attachement.zip

  • Hi Stephan,

    ok, let us have a look at the logs.  Do you only see this with the XDS510?  Only with one workspace or project?

    Best Regards,

    Lisa

  • Hi Lisa,

    we have only the XDS510USB.

    On the same PC when i use CCSV3 there is no problem. There is also no problem with sdflash or sdconfig.

    I have CCS 5.2 also installed on a Laptop for test and it is works good.

    Best regards,

    Stephan

  • Stephan,

    Some dlls are being picked up from your 3.3 install.  Can you check if your PATH environment variable contains any references to C:\CCSTudio_v3.3 and if so remove them?  3.3 should run fine without the PATH entries too - I don't know why they're even set in the first place.

    Darian

  • Hi Darin,

    thanks for fast and good help.

    This was the reason.

    Now the debug session starts correct.

    Best regards

    Stephan