Hi,
my CCS 5.2 crash after connecting the Spectrum Digital XDS510USB when i start the debug session.
Please can you check the attached log files.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
my CCS 5.2 crash after connecting the Spectrum Digital XDS510USB when i start the debug session.
Please can you check the attached log files.
Hi Lisa,
we have only the XDS510USB.
On the same PC when i use CCSV3 there is no problem. There is also no problem with sdflash or sdconfig.
I have CCS 5.2 also installed on a Laptop for test and it is works good.
Best regards,
Stephan
Stephan,
Some dlls are being picked up from your 3.3 install. Can you check if your PATH environment variable contains any references to C:\CCSTudio_v3.3 and if so remove them? 3.3 should run fine without the PATH entries too - I don't know why they're even set in the first place.
Darian
Hi Darin,
thanks for fast and good help.
This was the reason.
Now the debug session starts correct.
Best regards
Stephan