This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSV5 Debugger Crashes Easily and Often

Hello,

This bug is presented per the post "PLEASE READ FIRST: Code Composer Studio Forum Usage Guidelines"

A: The problem: The debugger crashes easily and often. 

1: We are using the latest version of CCS: 5.1.0.201206191800

2: We find some evidence in the forums of debugger crashes, but our situation renders the debugger pretty-much useless (so this seems unusual.)

3. OS: Windows 7 Enterprise, Service Pack 1

4. CCS: 5.1.0.201206191800

5. Emulator: SD XDS510 USB Plus Rev. B

6. A simple way to reproduce this is to press suspend (pause icon) and Resume (play icon, F8) a few times, resulting in the following windows message: “ccsstudio.exe has stopped working”.  We can easily reproduce this in a screenshare-type session upon request.

7. logs attached (not all of them, please ping if you need more info.

8. ccxml and gel files attached.

History:  We have been using CCSV4 with relative success with exactly the same computer, emulator, and hardware.  We do not have this kind of problem with CCSV4.  CCSV5 was installed over CCSV4.  There are no obvious cross-ups with environment variables. 

Thanks and Regards,

Steve

  • Steve,

    The log are missing from your post. Could you retry?  Any *.dmp files and a debug server log would be be most helpful.

  • This case is being follow-up offline. I'll provide an update when the cause is understood.

  • An issue has been identified with the call stack code on C55x. The problem is being tracked by SDSCM00045061 and a fix will be generally available in CCSv5.3.  Anyone else running into this problem on C55xx with CCS v5.2.1 should contact TI for a resolution.

  • I just upgraded to Code Composer Studio Version: 5.5.0.00077.  When I try to terminate the debugger or close the program altogether, it crashes.  If I subsequently forcefully close the program, it won't resume, claiming that the workspace is already in use.  I cannot re-run the project without rebooting the computer.  

    The target is an F2808 development board (dock); operating system is Windows 7 Enterprise Service Pack 1.

    Thank you for the help.  If you need log files or whatever, let me iknow.

    Ken