Hi,everyone!
I use ccs5.2 under win7 32-bit system and it works OK.But recently I install it under 64-bit system and there are some problems.
When I use simulator,it is still all right.But when I try to use the XDS560plus emulator,it often shows no respond .In detail,the debug session starts normally and there is no error information.But after the debug session is successfully launched and I set some breakpoints and trigger the program,the CCS5.2 often shows no respond.
I think the code is OK since it runs well when I use 32-bit system,is there anything else should be noticed when using ccs5 under 64-bit system or it do have some bugs because it is only for a 32-bit system?
Thanks,
zhao