Other Parts Discussed in Thread: MSP430F2274
Hi,
I am trying to install CCS 5.2 (beta) in Ubuntu for MSP430 microcontrollers following the installation instruction hat comes with the download. However I noticed during installation the "Select Emulators" window does not have the FET Emulator to select as the emulator I wanted.
The installation goes through and I can compile the code; however I cannot flash it to msp430 as it did not find the USB FET driver.
Alternatively I don't see the install_drivers.sh file under install_script/ folder as mentioned in the README_FIRST instruction file.
Am I missing anything in the installation process? Do I have to install the USB FET driver separately? If so where shall I get a driver for Linux which I can try out?
Thanks -Abhijit Das