Hi All,
I've just started learning Code Composer Studio and the EK-LM3S9D96. Exciting and daunting at the same time.
I thought the best way to learn would be to print out some examples and analyse them. I'm happy with 10 point font on screen, but when it comes to printing it's way too large. A better size would be 8 point. Totally legible and more code on the one page. I've learnt how to change font size so I can get by by setting the font size to 10 when I'm coding and 8 point when I'm printing and then back to 10 point. Pretty cumbersome.
I also find that the page margins are too large. There's 25 mm on the left, 15 mm on the right and a whopping 25 mm on top. This chews into the page payload.
So, my questions are:
1) Is it possible to set a different font type and size for printing versus on screen display?
2) Is it possible to set the print margins?
Thanks and Regards, Vito