This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538F512RKU Not an option Target option in Code Composer Studio

Other Parts Discussed in Thread: CC2538

I am running Windows 7 SP1 and have downloaded Code Composer 6.1.0. I am working on a school project using the cc2538DK and according to the BOM and the schematic the chip on the daughter board is a CC2538F512RKU. I downloaded CCS and included the cc2538 support files but I do not see an option for a CC2538F512RKU target. I have google CC2538F512RKU and only the schematic and BOM comes up. Is the CC2538F512RKU equivalent to a different target that is supported by  CCS?


Thanks,

Mark

  • Mark Richardosn said:
    I downloaded CCS and included the cc2538 support files but I do not see an option for a CC2538F512RKU target.

    Check the part number on the chip itself in the CC2538 Evaluation Module. The one in my kit is CC2538SF53, which is available as a device to select in CCS.