This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When attempting to install ccs 5.2 I receive the error "One or more features were not installed correctly. Please look at the log c:/Program Files /InstallJammerRegistry/........" No matter what method I choose to perform the installation I always receive the above error. Various ways I've attempted to install the application: (1) remove version 5.1.1 first, (2) install on a computer that never had an installation of ccs, (3) install on a computer with v5.1.1.1 but install v5.2 in a different folder. Any assistance is much appreciated.
K.D.
Hi,
could you please send us the installjammer registry contents? Have you tried redownloading?
Best Regards,
Lisa
Hi Lisa,
Here's the log file. I forgot to mention I'm installing ccs under Windows XP. I did not re-download ccs. In all of my attempts I used the same downloaded files.
6825.ccs_setup_5.2.1.00018_install.log
Thank you.
K.D.
Hi,
could you please do an md5 checksum on the downloaded zip file? You could also try downloading again. From the logs it looks like the installer had a problem with the emulation extraction.
Best Regards,
Lisa
Hello, I also am getting a similar problem I am getting a failed install with one or two features not being installed correctly. Here is my log file.
8662.ccs_setup_5.3.0.00090_install.log
Thank You,
Joseph Hoang
HI Joseph,
could you please try a fresh installation into c:/ti.
Best Regards,
Lisa