This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to create a CCS project with virtual folders from the command line. I have no issue linking in all the files I need but they create folders in my projects directory (which I do not want). This is what I currently see in CCS:
Here is an example of a project I made manually with virtual folders:
I noticed in the .project file for the correctly generated one they have some linked resources with <type>2</type> that represent the virtual folders. I am basically wanting to figure out how to create those when doing a command line project create.
Thanks for the help,
Zack L.
Zack,
I confirmed that creating virtual folders when using command line project create is currently not supported. If you believe this to be a useful functionality we could enter a enhancement request and add it for a future release. Let us know what you think.
Please file an enhancement request for this. I think this is an important feature for those trying to do automated project generation and want to link files without folders being created in the project directory.
Thanks,
Zack
Filed enhancement # SDSCM00045487, which can be tracked using the SDOWP link in my signature.