This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to create a CCS project with virtual folders from the command line. I have no issue linking in all the files I need but they create folders in my projects directory (which I do not want). This is what I currently see in CCS:
Here is an example of a project I made manually with virtual folders:
I noticed in the .project file for the correctly generated one they have some linked resources with <type>2</type> that represent the virtual folders. I am basically wanting to figure out how to create those when doing a command line project create.
Thanks for the help,
Zack L.
Zack,
I confirmed that creating virtual folders when using command line project create is currently not supported. If you believe this to be a useful functionality we could enter a enhancement request and add it for a future release. Let us know what you think.
Filed enhancement # SDSCM00045487, which can be tracked using the SDOWP link in my signature.