This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv5 profile clock cycle count C6713

I'm using CCSv5.2 and C6713 DSK. When I set up the profile clock it doesn't show an option to count instruction cycles. The default count option is branches. How can I count instruction cycles?

  • Under the Run->Clock->Setup option, you should be able to select different events to count. Once of them should be for cycles.

    What events do you see that are available?

    ki

  • Hi,

    I can see these options - clearly a different set from yours.

  • I was able to reproduce the issue using CCSv5.2.1 (I had originally used CCSv5.3.0). Those events definitely look off. Looks like it was a bug that has been fixed in 5.3.0. 5.3.0 is available for download if you wish to upgrade. However the patch update is not yet available and you;ll have to wait for it to get posted if you want to do an incremental update

    Thanks

    ki