Other Parts Discussed in Thread: OMAPL138
Hello,
I'm using CCS to develop a program to use on an OMAPL138 board. I have acquired the data and stored it in a float format on a variable array called calc_array. In the expressions window I can see the data acquired. But now I want to graph and it is not working. Keep in mind that I've graphed other arrays before, even this one on a previous version of CCS.
The problem I face is that I set my graph with the following attributes:
- Acquisition Buffer Size: 1024
- DSP Data Type: 32-bit floating point
- Index Increment: 1
- Q_value: 0
- Sampling Rate Hz: 1
- Start Address: calc_array
- Axis Display: True
- Data Plot Style: Line
- Display Data Size: 1024
- Grid Style: No Grid
- Magnitude Display Scale: Linear
- Time Display Unit: sample
- Use DC value for Graph: false