This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code Composer 4.2.4 - can't set multiple breakpoints, C28xx: Breakpoint Manager: Error programming AET Job

Other Parts Discussed in Thread: TMS320F2812

Hello,

I am using Code Composer Studio 4.2.4 with the XDS510 USB emulator and TMS320F2812 eZdSP board. I am unable to add more than one HW breakpoint in my code. When I try to add a second breakpoint, I get the following error:

C28xx: Breakpoint Manager: Error programming AET Job: This task cannot be accomplished with the existing AET resources.

I found a suggestion in similar threads to uncheck the "Enable CIO function use (requires setting a breakpoint)" option in the Generic Debugger Options menu. This has not resolved my problem. I have tried manually setting the breakpoints, and I have also tried using a GEL file to set the breakpoints (via the GEL_AddOutputFile() and GEL_AddInputFile() commands), but neither way has worked.

Are there any additional settings I can change that will allow me to set 2 HW breakpoints?

  • That setting (unchecking "Enable CIO function use") should allow you to set 2 hardware breakpoints. Do you have any other watchpoints or profile clock enabled that might be using up hardware resources?

    The other possibility is if you are using DSP/BIOS. In that case, one breakpoint would be used by default by the BIOS app. Please see this related thread for more information on that in case you are working with BIOS.

  • Hi Aarti, thanks for your response. I am not using DSP/BIOS, the profile clock, or other watchpoints. However, I was able to get a second HW breakpoint working. I created a new project and recompiled and re-loaded my code and the second HW breakpoint worked (even with "Enable CIO function use" checked). Thanks for the assistance.

  • Julie,

    Glad to hear and thanks for the update!