This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
It is fail when I compile C674x code. The fail message as follow:
js: "E:/CCSV4/xdctools_3_22_01_21/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: Error: Can't find platform package DSP.C674x gmake: *** [configPkg/compiler.opt] Error 1 gmake: Target `main-build' not remade because of errors.
How to solve to problem?
Regard,
Chen
Hi Chen,
are you using a remote drive or server? (I ask because I notice the E:). If so this could be one source of the problem. Are you using a scrtipt or running from the command line? A few further details to help clarify the context would help us to help you debug.
Best Regards,
Lisa
Hi Lisa,
I do not use a remote driver or server.It is the one problem when I compile the C647 code, and I do not use script or run from the command line, I just add the code to CCS4,2 abd then click "rebulid active project".
Thanks,
Chen
Hi Chen,
ok, glad to hear you found the issue and thanks for the update.
All the best with development.
Best Regards,
Lisa