This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
It is fail when I compile C674x code. The fail message as follow:
js: "E:/CCSV4/xdctools_3_22_01_21/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: Error: Can't find platform package DSP.C674x gmake: *** [configPkg/compiler.opt] Error 1 gmake: Target `main-build' not remade because of errors.
How to solve to problem?
Regard,
Chen
Hi Chen,
are you using a remote drive or server? (I ask because I notice the E:). If so this could be one source of the problem. Are you using a scrtipt or running from the command line? A few further details to help clarify the context would help us to help you debug.
Best Regards,
Lisa
Hi Lisa,
I do not use a remote driver or server.It is the one problem when I compile the C647 code, and I do not use script or run from the command line, I just add the code to CCS4,2 abd then click "rebulid active project".
Thanks,
Chen