This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TL;DR: Will this work?
Longer version: Running Code Composer 5.2 in Ubuntu 11.10. Trying to program an eZ430-RF256X development kit. I ran the driver installation script that came with Code Composer, and I've installed the appropriate udev rules. I get "MSP430: Error initializing emulator: No USB FET was found" whenever I try to debug a blinking LED program. Any suggestions or ideas?
EDIT: I guess as of April 2012, USB-FET was not supported in Linux, only the USB-UIF device is supported. Any updates since then?
Hi James,
I agree and myself am fully behind supporting these in Linux. I do believe support is coming, however if you would like an official statement I would post to the msp430 forum.
Best Regards,
Lisa