This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a problem to import a CCSv3.3 project into CCSv4. The steps I've followed are the next;
Open CCSv4
File>Import Legacy CCSv3.3 project>Select project file.
Once i've selected it, an error occurred:
!ERROR: java.lang.NullPointerException
at com.ti.common.managedbuild.core.util.CTIManagedBuildCoreUtils.getOptionDefiningSuperClass(CTIManagedBuildCoreUtils.java:824)
at com.ti.ccstudio.buildDefinitions.core.parser.BuildOptionParser.extractOptionName(BuildOptionParser.java:29)
at com.ti.ccstudio.managedbuild.core.legacy.LegacyProjectImporter.getOutputFileOptionSetting(LegacyProjectImporter.java:1640)
at com.ti.ccstudio.managedbuild.core.legacy.LegacyProjectImporter.processDependencies(LegacyProjectImporter.java:581)
at com.ti.ccstudio.managedbuild.core.legacy.LegacyProjectImporter.createManagedMakeProject(LegacyProjectImporter.java:447)
at com.ti.ccstudio.managedbuild.core.legacy.LegacyProjectImporter.doRun(LegacyProjectImporter.java:259)
at com.ti.ccstudio.managedbuild.core.legacy.LegacyProjectImporter.access$0(LegacyProjectImporter.java:211)
at com.ti.ccstudio.managedbuild.core.legacy.LegacyProjectImporter$1.run(LegacyProjectImporter.java:201)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:1737)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:1719)
at com.ti.ccstudio.managedbuild.core.legacy.LegacyProjectImporter.run(LegacyProjectImporter.java:199)
at com.ti.ccstudio.managedbuild.ui.wizards.importlegacy.ImportLegacyProjectWizard$1.run(ImportLegacyProjectWizard.java:107)
at org.eclipse.jface.operation.ModalContext$ModalContextThread.run(ModalContext.java:113)
I have migrated some projects and i haven't got any problem. The fact is that this one is the only project with project dependences:
; Code Composer Project File, Version 2.0 (do not modify or remove this line)
[Project Settings]
ProjectDir="E:\JP\WorkingFolder\CodeInReleaseMode\VolumeChangeMultilangVer5.0\Drivers\KeyPad\System\"
ProjectType=Library
CPUFamily=TMS320C55XX
Tool="Archiver"
Tool="Compiler"
Tool="CustomBuilder"
Tool="DspBiosBuilder"
Config="Debug"
Config="Release"
[Project Dependencies]
Source="..\..\GPIO\System\gpiodrv.pjt"
["..\..\GPIO\System\gpiodrv.pjt" Settings]
MatchConfigName=true
[Source Files]
Source="..\Source\Drv_Keypad.c"
["Archiver" Settings: "Debug"]
Options=-r -o".\Debug\keypad.lib"
["Archiver" Settings: "Release"]
Options=-r -o".\Release\keypad.lib"
["Compiler" Settings: "Debug"]
Options=-g -mg -pdsw225 -fr"$(Proj_dir)\Debug" -i"$(Proj_dir)\..\Include" -i"$(Proj_dir)\..\..\..\CSL\Include" -i"$(Proj_dir)\..\Source" -i"$(Proj_dir)\..\..\..\CSL\Source" -i"$(Proj_dir)\" -i"$(Proj_dir)\..\..\i2c\Include" -i"$(Proj_dir)\..\..\..\PSP\inc" -i"$(Proj_dir)\..\..\..\PSP\pal_os\inc" -i"$(Proj_dir)\..\..\..\PSP\pal_sys\inc" -i"$(Proj_dir)\..\..\..\PSP\soc\inc" -i"$(Proj_dir)\..\..\common" -i"$(Proj_dir)\..\..\..\..\Drivers\KeyPad\System\" -i"$(Proj_dir)\..\..\Drivers\i2c\Include" -i"$(Proj_dir)\..\..\..\Global\Common\Include" -i"$(Proj_dir)\..\..\GPIO\Include" -i"$(Proj_dir)\..\..\..\SYSMgr\System" -i"$(Proj_dir)\..\GPIO\Include" -ml -v5505
["Compiler" Settings: "Release"]
Options=-pdsw225 -fr"$(Proj_dir)\Release" -i"$(Proj_dir)\..\Include" -i"$(Proj_dir)\..\..\..\CSL\Include" -i"$(Proj_dir)\..\Source" -i"$(Proj_dir)\..\..\..\CSL\Source" -i"$(Proj_dir)\" -i"$(Proj_dir)\..\..\i2c\Include" -i"$(Proj_dir)\..\..\..\PSP\inc" -i"$(Proj_dir)\..\..\..\PSP\pal_os\inc" -i"$(Proj_dir)\..\..\..\PSP\pal_sys\inc" -i"$(Proj_dir)\..\..\..\PSP\soc\inc" -i"$(Proj_dir)\..\..\common" -i"$(Proj_dir)\..\..\..\..\Drivers\KeyPad\System\" -i"$(Proj_dir)\..\..\Drivers\i2c\Include" -i"$(Proj_dir)\..\..\..\Global\Common\Include" -i"$(Proj_dir)\..\..\GPIO\Include" -i"$(Proj_dir)\..\..\..\SYSMgr\System" -i"$(Proj_dir)\..\GPIO\Include" -ml -v5505
["DspBiosBuilder" Settings: "Debug"]
Options=-Dconfig.importPath="C:\Archivos de programa\Texas Instruments\bios_5_42_00_07\packages;"
I hope you can help me,
Best regards,