This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi;
when i try to build a project with grace it get these errors:
Description Resource Path Location Type
#10010 errors encountered during linking; "servo.out" not built servo C/C++ Problem
<a href="file:/C:/ti/ccsv5/tools/compiler/dmed/HTML/10234.html">#10234-D</a> unresolved symbols remain servo C/C++ Problem
unresolved symbol Grace_init, first referenced in ./main.obj servo C/C++ Problem
#10008-D cannot find file "./configPkg/linker.cmd" servo C/C++ Problem
any suggestions with these errors??
i am workig with mps430g2211 and CCSv5.3.0.00090
Thanks
Erdem
Hi Erdem,
unresolved symbol errors are typical when a library is missing (ie ccs is not properly directed to the library). Please see this wiki:
http://processors.wiki.ti.com/index.php/Include_paths_and_options
Is this an unmodified project/example?
Best Regards,
Lisa
First, thanks for quick reply.
The code i am trying to build, generated by grace itself. there is no modification over it.
Also, i checked everywhere but i can not find this directory or file "./configPkg/linker.cmd". Is it possible that my installation of CCS somewhat broken or faulty??
This file is located in the project directory, not in the CCS installation directory.
Since you said everything was left on default, your project or project workspace could be corrupted. I would recommend to start with a new workspace from scratch and see if the problem persists. If it does, a clean reinstall of CCS is recommended.
Of course, before you try that, do a "clean" of your project, maybe this is enough.
Kind regards,
Michael
i reinstalled ccs but it didint solve my problem.
When i try to build codes without grace, they go fine.no build errors. It is something about grace i think
Thanks again
Erdem
Hello Erdem,
Did you try to do your configuration again in a new project in a new workspace?
Can you attach the project if the problem persists?
Thanks,
Michael