Dear All,
we are facing some linker problem., memory sections are defined in our linker.cmd file is like this
IROM 11700000 00100000 00000000 00100000 R X
CFGIRAM1 11800000 00000200 000001a0 00000060 RW X
CFGIRAM2 11800200 00000600 00000000 00000600 RW X
IRAM 11800800 0003fa00 00035823 0000a1dd RW X
L1PSRAM 11e00000 00008000 00000000 00008000 RW X
L1DSRAM 11f00000 00008000 00000000 00008000 RW
L3_CBA_RAM 80000000 00020000 00000000 00020000 RW X
DDR2_DATA c0000000 00500000 00004800 004fb800 RW X
DDR2_CODE c0500000 00500000 00012740 004ed8c0 RW X
object files are created for every file containing in project but unable to map in .MAP file for some files, if any function called from those files, compiler will through error like this.
undefined first referenced
symbol in file
--------- ----------------
_BootInit ./Application/boot_6746_A.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking;
"../../../Out/ss4_main_1_10.out" not built
>> Compilation failure
gmake: *** [../../../Out/ss4_main_1_10.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
help me out
With regards,
Ravi