Does the Code Composer Compiler automatically create a symbol which indicates which controller is used?
I have to set the Controller in the Project Properties of Code Composer Studio. So it should be possible that the compiler creates a symbol like the PART_LM<XXXXXX> symbols which is used in the StellarisWare.
I can set the symbol manually. But then I have to change it in two places which is not so nice.
Thanks and Regards
Markus