Hi
We are developing for the TCI6618 device using CCS 5.3. In the target configuration file, which cores should run the gel file evmc6670l.gel?
Is it sufficient / typical for just core 0 to run the gel file?
BR
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
We are developing for the TCI6618 device using CCS 5.3. In the target configuration file, which cores should run the gel file evmc6670l.gel?
Is it sufficient / typical for just core 0 to run the gel file?
BR
David
Hi David,
By just looking at the GEL file, it looks like there is both CPU level and Device/Board level initialization being done. For the latter, I'd imagine only core 0 would have to run since that initialization would apply to the whole device. But the CPU level stuff you'd want each core to execute it.
But i am hardly a C66x expert so I may be misinterpreting what some of the GEL actions do. I would also check in the C66x forums, they would understand the initialization needed and what the GEL file is doing.
Thanks
ki