Hello everyone,
I am new to the MSP430. I have just bought one to help my sister build an automated home gardening display for a science exhibition.
I have installed the CCS (Version 5.4.0.00091) on Windows 7 (32-bit) and I have tried the first LED blinking project.
But, it seems that I am having the same problem that many here had:
**** Build of configuration Debug for project Temp ****
"D:\\\\ccsv5\\utils\\bin\\gmake" -k all
'C:\Users\ZAK' is not recognized as an internal or external command,
operable program or batch file.
The system cannot find the path specified.
gmake: *** [blink.obj] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
I have tried their many solutions, but with no success.
While debugging, the message that pops up is:
Load program error: Encountered a problem loading file: D:/Launchpad_Projects/Temp/Debug/Temp.out
Could not open file.
Your help would be greatly welcomed.
Thanks
Zakhir