Hi,
I need to debug a board using TMS32C032. I have the emulator (USB) and using CC C3x C4x software. But when I open the Code Composer, I got an error.
Can't Initialize Target DSP
I/O Port = 240
Board Name: sdgo3x
Cpu name: CPU
What should I do to solve this problem. I'm new to DSP.
Note: The Driver should be ok as I did check the hardware in Microsoft Control Panel.
The Emulator has powered from the target board.
I'm using MPSD. The wring should be fine. PD has 5V
Thanks.