Hi,
I'm a part time post graduate student and the University loaned 1 set of the above mentioned DSK to each and every student in the class.
I'm running Windows 8 (64 bit) and I do not have access to any other OS. The oldest OS in the university runs on Windows 7.
I used the cd that came with the DSK and installed CCS via the full install. The kit came with a direct usb cable to connect the board directly to my pc (not JTAG). The installation guide said that leaving the installation cd in the drive would be sufficient for letting the board detect the driver in it to properly install itself. I took the guide's word for it.
The board powers on fine. i.e. LEDs flash and stay on.
After installing it, I tried to run CCS and got the following error:
http://i269.photobucket.com/albums/jj58/Dethyl/frustration.png
Checking the usb cable and power cable with other devices and they were fine. I checked my hardware settings and I obtained this information.
http://i269.photobucket.com/albums/jj58/Dethyl/frustration2.png
Looks like it wasn't installed. Odd....
I tried updating the driver but they couldn't find it on the internet. I chose manual location (the cd drive where the installation disk was loaded) and the PC said it couldn't find the usb driver in the cd.
Please advise? I'm not sure what other information I should provide.