This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I try to debug on my BBB using OpenOCD (connector is already mounted on lower side of the board and OpenOCD-USB probe connected). Unfortunately I run into two problems. After starting OpenOCD with
arm-none-linux-gnueabi-gdb
I get some messages
Open On-Chip Debugger 0.7.0 (2013-05-22-13:14) Licensed under GNU GPL v2 For bug reports, read http://openocd.sourceforge.net/doc/doxygen/bugs.html Info : only one transport option; autoselect 'jtag' adapter speed: 16000 kHz trst_and_srst separate srst_gates_jtag trst_push_pull srst_open_drain connect_deassert_srst Warn : unable to open ftdi device (trying more): device not found Info : clock speed 6000 kHz Info : JTAG tap: am335x.jrc tap/device found: 0x1b94402f (mfg: 0x017, part: 0xb944, ver: 0x1) Info : JTAG tap: am335x.dap enabled Info : am335x.cpu: hardware has 6 breakpoints, 2 watchpoints Error: JTAG-DP STICKY ERROR Error: MEM_AP_CSW 0x80000042, MEM_AP_TAR 0x80001140 Error: JTAG-DP STICKY ERROR Error: MEM_AP_CSW 0x80000042, MEM_AP_TAR 0x80001140 Error: JTAG-DP STICKY ERROR Error: MEM_AP_CSW 0x80000042, MEM_AP_TAR 0x80001140 Error: JTAG-DP STICKY ERROR Error: MEM_AP_CSW 0x80000042, MEM_AP_TAR 0x80001140 Error: JTAG-DP STICKY ERROR Error: MEM_AP_CSW 0x80000042, MEM_AP_TAR 0x80001150 Error: JTAG-DP STICKY ERROR Error: MEM_AP_CSW 0x80000042, MEM_AP_TAR 0x80001150 Error: JTAG-DP STICKY ERROR Error: MEM_AP_CSW 0x80000042, MEM_AP_TAR 0x800011c0 Error: JTAG-DP STICKY ERROR Error: MEM_AP_CSW 0x80000042, MEM_AP_TAR 0x800011c0
Looks like it connects to BBB but has some problems?
Next when I try to configure OpenOCD in CCS I chosse "OpenOCD (via pipe)" in debug setting / Debugger. Amazingly the predefined "GDB Command" there is simply "gdb". Shouldn't that be an ARM-GDB? Or a TI-specific GDB since my code is compiled with the TI-compiler?
When I ignore these problem and try to load a program to BBB I get an error message in CCS and OpenOCD shows following output:
Error: ftdi_write_data: usb bulk write failed Error: couldn't write MPSSE commands to FT2232 Polling target am335x.cpu failed, GDB will be halted. Polling again in 100ms Error: ftdi_write_data: usb bulk write failed Error: couldn't write MPSSE commands to FT2232 Polling target am335x.cpu failed, GDB will be halted. Polling again in 300ms Error: ftdi_write_data: usb bulk write failed Error: couldn't write MPSSE commands to FT2232 Polling target am335x.cpu failed, GDB will be halted. Polling again in 700ms Error: ftdi_write_data: usb bulk write failed Error: couldn't write MPSSE commands to FT2232 Polling target am335x.cpu failed, GDB will be halted. Polling again in 1500ms Error: ftdi_write_data: usb bulk write failed Error: couldn't write MPSSE commands to FT2232 Polling target am335x.cpu failed, GDB will be halted. Polling again in 3100ms Error: ftdi_write_data: usb bulk write failed Error: couldn't write MPSSE commands to FT2232 Polling target am335x.cpu failed, GDB will be halted. Polling again in 6300ms Error: ftdi_write_data: usb bulk write failed Error: couldn't write MPSSE commands to FT2232 Polling target am335x.cpu failed, GDB will be halted. Polling again in 6300ms
Any help is appreciated :-)
Hi,
We do not support OpenOCD in CCS (nor are very familiar with it), therefore you will have better chances if you contact the experts either on the device forum or any OpenOCD discussion forum throughout the internet.
That said, I have just one remark: TI compilers do not generate Linux-compatible code but instead "baremetal", therefore the arm-none-linux-gnueabi-gdb will not understand what the code does in the target, as it expects a Linux environment.
Obviously this remark stems from my lack of knowledge of OpenOCD, which may possibly have a Linux distro built into the emulation dongle and therefore accept standard Linux GDB commands from the host and translate them to be used in a device running "baremetal" code.
Regards,
Rafael