Other Parts Discussed in Thread: TMS320VC5510A
I'm using CCS 4. I am in the process of porting a CCS 3.3 project over. I need to include the chip support libraries, and am having trouble doing so. I have downloaded and installed them from TI's website. I have updated the compiler "include options" to include the path with the new path for the CSL include. I also added the .lib file to the linker options.
The CSL header files now show up in my project's include folder, as well as the compiler options screen. But when I build the project, the compiler does not look in the specified directory, and I end up with errors that it can't find the specified header files.
I have tried cleaning the workspace, that didn't help.
IDE is CCS 4.0.1.01001
Code generation tools 4.3.2
DSP/BIOS 5.40.02.22