I'm using F28335 experimenter kit (with XDS100) and working with real time mode debug.
It happens quite often that CCSv4 crashed (terminates). When I relaunch it the Emulator is unable to connect to the target.
Error connecting to the target:
Error 0x80000200/-1142
Fatal Error during: OCS,
Processor blocked debug accesses.
Even if I try to un-power and re-power the DSP board, still the same error.
I launch CCSv3.3 and I can connect to the target and reset the CPU.
However If I re-lauch CCSv4, I still have the same error message. Only solution is to restart computer.
As I can connect with CCSv3.3 it is a pure CCSv4 issue. How can I send the infos to TI to help them debug/improve CCSv4 ?
One more point. As I said I am able to connect and do things with CCSv3.3 and not in CCSv4. Even though it says "Processor blocked debug accesses" it is a CCSv4 issue. I've found that using Scripts "Full_Halt_With_Reset" removes the error. This sounds weird to me as the CPU is already halted and reset using CCSv3.3.
Perhaps it's a minor issue problem, but I thought it was important to tell other user, because as I spend quite a lot of time finding the solution as I thought it was a problem with the DSP and not with CCSv4